SLAU923B June 2025 – April 2026 MSPM0H3215 , MSPM0H3216 , MSPM0H3216-Q1
The input glitch filter can be enabled by setting the TIMx. IFCTL_01[0/1].FE bit. The filter period is configured by setting the TIMx. IFCTL_01[0/1].FP bit.
A consecutive period or majority voting format selected by the TIMx.IFCTL_xy[0/1].CPV bit is used to select the criteria for a CCP input signal.
The example shown in Figure 17-13 shows the difference between consecutive period and majority voting formats with a digital filter implemented to capture a CCP input signal of 3 TIMCLK periods.