SLAA870 February 2019 AFE7422 , AFE7444
The next experiment characterizes the time required for DAC A on the AFE74xx to hop from 10 MHz to 100 MHz using a maximum SPI clock of 39.4 MHz to reprogram a single 32-bit NCO. Figure 12 shows the test setup for measuring the hop time when updating the frequency in a single NCO. The output of DAC A on the AFE74xxEVM (AFE7422EVM or AFE7444EVM) is connected to the channel 1 input of an oscilloscope. Channel 2 of the oscilloscope is connected to SDEN SPI pin, which indicates the start of the SPI write sequence.
Figure 12. Test Setup for Measuring Hop Time From 10 MHz to 100 MHz