SLAA870 February 2019 AFE7422 , AFE7444
Figure 17 shows that the time required to switch from TXNCO0 (100 MHz) to TXNCO1 (10 MHz) is approximately 658 ns from the issuance of the command through the SPI clock of approximately 40 MHz
Figure 17. Hop Time When Switching From One NCO to Another is Approximately 658 ns