SLAA870 February 2019 AFE7422 , AFE7444
Direct digital synthesis (or DDS) mode is a technique to generate an analog signal at a frequency specified by a digital code. The AFE74xx supports DDS mode where the DAC outputs a constant analog signal at a frequency specified by the 32-bit accumulator word of the active TX NCO. Each DAC can operate in DDS mode independent of all other DACs. For example, it is possible to transmit a modulated waveform on DAC A and DAC C, while DDS mode is enabled in DAC B and DAC D. DDS mode is enabled by navigating to the Configuration tab in the AFE74xx GUI and selecting on in the constant tone drop-down menu of the respective DAC, as shown in Figure 7.
Figure 7. Enabling DDS Mode in DAC A Although each DAC contains two NCOs, TXNCO0 is the selected by default and is programmed to 1700 MHz. Therefore, when DDS mode is enabled, the DAC A output signal is 1700 MHz. Figure 8 shows the output of DAC A on a spectrum analyzer.
Figure 8. DAC A Output of 1700 MHz in DDS Mode