SFFSAY3 January 2026 F29H850TU , F29H859TU-Q1 , TMCS1123 , TMCS1123-Q1 , TPS650362-Q1 , TPS650365-Q1
DFA should be performed to identify the cascaded failures and common-cause failures that could influence redundancy. Additional TSRs for independence requirement are recognized by DFA analysis. Generally, DFA analysis confirms:
For example, if the bias supply of MCU is short-circuited to ground, the plausibility check cannot detect the fault, and software-related safety mechanisms also lose its function. In this case, voltage monitoring is the critical safety mechanism to verify the OBC enters safe state.