SBAU213A September   2013  – July 2020 ADS8860

 

  1.   Trademarks
  2. 1EVM Overview
    1. 1.1 ADS8860EVM Kit
    2. 1.2 ADS8860EVM Board
  3. 2EVM Analog Interface
    1. 2.1 ADC Drive Amplifier and Filter
    2. 2.2 Reference Drive
  4. 3Digital Interface
    1. 3.1 Serial Interface (SPI)
    2. 3.2 I2C Bus for the Onboard EEPROM
  5. 4Power Supplies
  6. 5ADS8860EVM Initial Setup
    1. 5.1 Software Installation
  7. 6EVM Operation
    1. 6.1 Connecting the Hardware
    2. 6.2 Using the Optional Precision Signal Injector (PSI)
    3. 6.3 EVM GUI Global Settings for ADC Control
    4. 6.4 Time Domain Display
    5. 6.5 Frequency Domain Display
    6. 6.6 Histogram Display
  8. 7Bill of Materials, Schematics, and Layout
    1. 7.1 Bill of Materials
    2. 7.2 Board Layouts
    3. 7.3 Schematics
  9. 8Reference
  10. 9Revision History

Connecting the Hardware

Connect the EVM as shown in Figure 6-1 after installing the software:

  1. Physically connect P2 of the PHI to J2 of the ADS8860EVM. Install the screws to assure a robust connection.
  2. Connect the USB on the PHI to the computer first.
    • LED D5 on the PHI lights up, indicating that the PHI is powered up
    • LEDs D1 and D2 on the PHI start blinking to indicate that the PHI is booted up and communicating with the PC; Figure 6-1 shows the resulting LED indicators
  3. Start the software GUI as shown in Figure 6-2. Notice that the LEDs blink slowly while the FPGA firmware is loaded on the PHI. This process takes a few seconds, then the AVDD and DVDD power supplies turn on.
  4. Connect the signal generator. The input range is 0 V to 5 V. A common input signal applied is a 4.9-VPP signal with a 2.5-V offset. This signal is adjusted just below the full-scale range to avoid clipping.

GUID-C8129EDB-9923-44B4-A0B1-8B103CFEBAA1-low.gifFigure 6-1 ADS8860EVM Hardware Setup and LED Indicators
GUID-FB94AF31-1065-4654-9DEE-6407A5831F21-low.gifFigure 6-2 Launch the EVM GUI Software