SBAU213A September 2013 – July 2020 ADS8860
The PHI provides multiple power-supply options for the EVM, derived from the USB supply of the computer. The EEPROM on the ADS8860EVM uses a 3.3-V power supply generated directly by the PHI. The EVM_REG_5V5 is a 5.5-V supply from the PHI and is applied to the input of two LDOs to generate other supplies on the EVM. The analog supply of the ADC (AVDD = 3.3 V) is powered by the TPS7A4700RGWR (U11) LDO. A 5.3-V supply is also generated using TPS7A4700RGWR (U9) LDO. This supply powers the voltage reference (U2) and amplifier (U4). The ADC digital supply (DVDD = 3.3 V), is generated by the PHI. Three LEDs are connected to the 5.3-V, AVDD, and DVDD supplies. These LEDs illuminate after the software GUI loads and the PHI turns on its output power supplies.
Figure 4-1 Power Supplies, Regulators, and Indicators