SBAU213A September 2013 – July 2020
The time domain display tool allows visualization of the ADC response to a given input signal. This tool is useful for both studying the behavior and debugging any gross problems with the ADC or drive circuits. The user can trigger data capture of the selected number of samples from the ADS8860EVM, as per the current interface mode settings indicated in Figure 6-5 by using the Capture button. The sample indices are on the x-axis and there are two y-axes showing the corresponding output codes as well as the equivalent analog voltages based on the specified reference voltage. Switching pages to any of the Analysis tools described in the subsequent sections causes calculations to be performed on the same set of data.
Figure 6-5 Time Domain Display Tool Options