DLPU094 July 2020 DLP5530S-Q1
The DLPC230S-Q1 stores an error history to indicate which errors have occurred in the system. The error history can be read by the host MCU via SPI or I2C. Full implementation details of the Error History, including error codes are described in the DLPC230S-Q1 Programmer's Guide For Display Applications.