7.3.2.2.1 Communication Interface and Register Protection
The following methods are used to protect communication between ICs in the system and the data stored in critical registers.
- [SM_14] Host Command CRC: A CRC check on the incoming host commands to detect corrupted commands. Protects against incorrect dimming value being set due to a corrupted command
- [SM_15] Loss Of Dimming Command Test: Checks that dimming commands are regularly being received from the host. This enures that communication with the host has not been lost. If communication with the host is lost, and old dimming value may create an image that is too bright for the current driving conditions. The host can configure a timer within which the DLPC230S-Q1 should receive a dimming command. If the command is not received within this timing the test fails. A default value for the timer can also be configured in flash. Upon failure, emergency shutdown will be executed and an error will be logged.
- [SM_16] TPS9000S-Q1 Interface Signal Connection Test: Checks the SPI and the LED select interfaces between the DLPC230S-Q1 and TPS99000S-Q1. Checks SPI interface by writing to a dedicated register and reading back the value. Checks the LED select interface by sending LED select signals and reading back the LED select values from the TPS99000S-Q1 via SPI. This test can be configured to run at start-up, and it can be executed by command after the software is changed to Stand-by mode via host command. Upon failure, software will not transition Display Mode even if it is commanded by the host. An error will also be logged.
- [SM_17] DLPC230S-Q1 to TPS99000S-Q1 SPI Byte-Wise Parity: The DLPC230S-Q1 to TPS99000S-Q1 SPI interface implements a byte-wise parity for detecting command or data corruption. The DLPC230S-Q1 sends a parity bit with the payload for any read or write from the TPS99000S-Q1 registers. If the TPS99000S-Q1 detects a parity error it will indicate a parity error to the DLPC230S-Q1 via a status bit. Register writes to the TPS99000S-Q1 will not be performed if a parity error is detected. If the DLPC230S-Q1 detects three consecutive frames of parity error, it will not reset the DLPC230S-Q1 Processor Watchdog Timer (WD1). This will result in an emergency shutdown. An error code will also be logged.
- [SM_18] DLPC230S-Q1 to TPS99000S-Q1 ADC Interface SPI Parity: The DLPC230S-Q1 to TPS99000S-Q1 implements a parity check to ensure that ADC measurement commands and data are not corrupted. Parity is implemented on both the read command transaction and on the return data. Each command transaction from the DLPC230S-Q1 to TPS99000S-Q1 includes a start bit, the command id, the command id repeated, a parity bit, and a stop bit. The repeated command and data bytes must match and the parity bit must be correct. Additionally, the data returned from the TPS99000S-Q1 to DLPC230S-Q1 includes 12 data bits, 3 error bits, 12 data bits repeated, 3 error bits repeated, and 1 parity bit. The two copies of the 12-bit data, and the two copies of the 3-bit error codes must match. Additionally, the parity bit must be correct. If the TPS99000S-Q1 detects a parity error, it will indicate the error to the DLPC230S-Q1 via a status bit. If 3 consecutive errors are detected, the test fails. Upon failure, emergency shutdown will be executed and an error will be logged.
- [SM_19] TPS99000S-Q1 Password Protected Register Space: A portion of the TPS99000S-Q1 register space is protected by a password. The DLPC230S-Q1 unlocks this register space by writing the password before updating these registers. After updating these registers, the DLPC230S-Q1 locks this register space.
- [SM_20] TPS99000S-Q1 Register Checksum: The TPS99000S-Q1 implements a checksum on functionally grouped registers. This checksum is used to detect bit level changes occurring due to random events. When the DLPC230S-Q1 updates any TPS99000S-Q1 registers, it updates the checksum for that group. The TPS99000S-Q1 periodically calculates a checksum on each group of registers and compares it to the last checksum stored by the DLPC230S-Q1. If the TPS99000S-Q1 detects a checksum error, it sets a status bit that can be read by the DLPC230S-Q1 via SPI. If an error is detected, the DLPC230S-Q1 will attempt to re-write the registers and checksum up to three times. If the error persists after three attempts, an emergency shutdown will be executed and an error will be logged.