ZHCSG69E November 2016 – May 2018 DM505
PRODUCTION DATA.
VREF (ddrx_vref0) is used as a reference by the input buffers of the DDR2 memories. VREF is intended to be half the DDR2 power supply voltage and should be created using a resistive divider as shown in Figure 7-39. Other methods of creating VREF are not recommended. Figure 7-42 shows the layout guidelines for VREF.
Figure 7-42 VREF Routing and Topology