ZHCSNA1A april 2020 – february 2021 BQ25968
PRODUCTION DATA
A typical application consists of the device configured as an I2C controlled parallel charger along with a standard switching charger, however, it can also be used with a linear charger or PMIC with integrated charger as well. For simplicity, it is called the primary charger. As shown in Figure 9-2 the device can start fast charging after the primary charger completes precharging, where the BQ25890 is used as the primary charger. The device will then hand back charging to the primary charger when final current tapering is desired. This point is usually where the efficiency of the primary charger is acceptable for the application. The device can be used to charge Li-ion and Li-polymer batteries used in a wide range of smartphones and other portable devices. To take advantage of the high charge current capabilities of the BQ25968, it may be necessary to charge in excess of 1C. In this case, be sure to follow the battery manufacturers recommendations closely.