ZHCSSI3 February 2024 ADS1288
PRODUCTION DATA
The WREG command writes register data. The command is two bytes followed by the designated number of register bytes to be written. The ADC auto-increments the address up to the number of registers specified in the command. The incrementing address does not wrap. The first byte of the command is the opcode added to the register starting address, and the second byte is the number of registers to write minus one.
Figure 7-27 shows an example of a three-register write operation starting at register address 01h.