ZHCS065G March 2011 – January 2024 DAC3482
PRODUCTION DATA
Register Name | Address | Bit | Name | Function | Default Value |
---|---|---|---|---|---|
config5 | 0x05 | 15 | alarm_from_zerochk | This alarm indicates the 8-bit FIFO write pointer address has an all zeros patterns. Due to pointer address being a shift register, this is not a valid address and will cause the write pointer to be stuck until the next sync. This error is typically caused by timing error or improper power start-up sequence. If this alarm is asserted, resynchronization of FIFO is necessary. Refer to Section 6.5.1 for more detail. | NA |
14 | Reserved | Reserved for factory use. | NA | ||
13:11 | alarms_from_fifo(2:0) | Alarm indicating FIFO pointer collisions and nearness: 000: All fine 001: Pointers are 2 away 01x: Pointers are 1 away 1xx: FIFO pointer collision If the FIFO pointer collision alarm is set when collisiongone_ena is enabled, the FIFO must be re-synchronized and the bits must be cleared to resume normal operation. | NA | ||
10 | alarm_dacclk_gone | Alarm indicating the DACCLK has been stopped. If the bit is set when dacclkgone_ena is enabled, the DACCLK must resume and the bit must be cleared to resume normal operation. | NA | ||
9 | alarm_dataclk_gone | Alarm indicating the DATACLK has been stopped. If the bit is set when dataclkgone_ena is enabled, the DATACLK must resume and the bit must be cleared to resume normal operation. | NA | ||
8 | alarm_output_gone | Alarm indicating either alarm_dacclk_gone, alarm_dataclk_gone, or alarm_fifo_collision are asserted. It controls the output. When high it will output 0x8000 for each output connected to the DAC. If the bit is set when dacclkgone_ena, dataclkgone_ena, or collisiongone_ena are enabled, then the corresponding errors must be fixed and the bits must be cleared to resume normal operation. | NA | ||
7 | alarm_from_iotest | Alarm indicating the input data pattern does not match the pattern in the iotest_pattern registers. When data pattern checker mode is enabled, this alarm in register config5, bit 7 is the only valid alarm. Other alarms in register config5 are not valid and can be disregarded. | NA | ||
6 | Reserved | Reserved for factory use. | NA | ||
5 | alarm_from_pll | Alarm indicating the PLL has lost lock. For version ID 100b or earlier, alarm_from_PLL may not indicate the correct status of the PLL. Refer to pll_lfvolt(2:0) in register config24 for proper PLL lock indication. | NA | ||
4 | alarm_rparity | Alarm indicating a parity error on data captured on the rising edge of DATACLKP/N. | NA | ||
3 | alarm_fparity | Alarm indicating a parity error on data captured on the falling edge of DATACLKP/N. | NA | ||
2 | alarm_frame_parity | Alarm indicating a parity error when using the FRAME as parity bit. | NA | ||
1 | Reserved | Reserved for factory use. | NA | ||
0 | Reserved | Reserved for factory use. | NA |