ZHCSJ34F December 2015 – May 2019 TDA2HG , TDA2SG , TDA2SX
PRODUCTION DATA.
NOTE
For more information, see the Initialization (ROM Code) section of the device TRM.
| SIGNAL NAME | DESCRIPTION | TYPE | BALL |
|---|---|---|---|
| sysboot0 | Boot Mode Configuration 0. The value latched on this pin upon porz reset release will determine the boot mode configuration of the device. | I | M6 |
| sysboot1 | Boot Mode Configuration 1. The value latched on this pin upon porz reset release will determine the boot mode configuration of the device. | I | M2 |
| sysboot2 | Boot Mode Configuration 2. The value latched on this pin upon porz reset release will determine the boot mode configuration of the device. | I | L5 |
| sysboot3 | Boot Mode Configuration 3. The value latched on this pin upon porz reset release will determine the boot mode configuration of the device. | I | M1 |
| sysboot4 | Boot Mode Configuration 4. The value latched on this pin upon porz reset release will determine the boot mode configuration of the device. | I | L6 |
| sysboot5 | Boot Mode Configuration 5. The value latched on this pin upon porz reset release will determine the boot mode configuration of the device. | I | L4 |
| sysboot6 | Boot Mode Configuration 6. The value latched on this pin upon porz reset release will determine the boot mode configuration of the device. | I | L3 |
| sysboot7 | Boot Mode Configuration 7. The value latched on this pin upon porz reset release will determine the boot mode configuration of the device. | I | L2 |
| sysboot8 | Boot Mode Configuration 8. The value latched on this pin upon porz reset release will determine the boot mode configuration of the device. | I | L1 |
| sysboot9 | Boot Mode Configuration 9. The value latched on this pin upon porz reset release will determine the boot mode configuration of the device. | I | K2 |
| sysboot10 | Boot Mode Configuration 10. The value latched on this pin upon porz reset release will determine the boot mode configuration of the device. | I | J1 |
| sysboot11 | Boot Mode Configuration 11. The value latched on this pin upon porz reset release will determine the boot mode configuration of the device. | I | J2 |
| sysboot12 | Boot Mode Configuration 12. The value latched on this pin upon porz reset release will determine the boot mode configuration of the device. | I | H1 |
| sysboot13 | Boot Mode Configuration 13. The value latched on this pin upon porz reset release will determine the boot mode configuration of the device. | I | J3 |
| sysboot14 | Boot Mode Configuration 14. The value latched on this pin upon porz reset release will determine the boot mode configuration of the device. | I | H2 |
| sysboot15 | Boot Mode Configuration 15. The value latched on this pin upon porz reset release will determine the boot mode configuration of the device. | I | H3 |