ZHCADP2A January   2024  – November 2025 AM3351 , AM3352 , AM3354 , AM3356 , AM3357 , AM3358 , AM3358-EP , AM3359 , AM4372 , AM4376 , AM4377 , AM4378 , AM4379 , AM623 , AM625 , AM625SIP , AM62A1-Q1 , AM62A3 , AM62A7 , AM62L , AM62P , AM6411 , AM6412 , AM6421 , AM6422 , AM6441 , AM6442

 

  1.   1
  2.   摘要
  3.   商标
  4. 1简介
  5. 2当前设计
  6. 3支持
  7. 4演示
  8. 5总结
  9. 6参考资料
  10. 7修订历史记录

支持

在演示中,我们使用了 AM62P 和 AM62L。一般情况下,可以使用任何支持 Linux 并可连接网络的 SoC。如需更多信息,请参阅:AM62P 和 AM62L。关于软件,可按照以下步骤在主机 PC 上进行交叉编译:

  1. 在 Ubuntu 主机上,下载并安装与您要使用的内核版本相对应的 SDK,例如:AM62L 11.00 SDK 安装程序。

  2. 使用以下命令,解压缩 SDK 中的 rootfs:

    cd <SDK Install Path>/filesystem/<device>
    tar -xf tisdk-default-image-am62lxx-evm.rootfs.tar.xz -C temp/

    妥善留存此解压缩目录的路径。

  3. 使用以下命令,克隆并更新 Matter 存储库:

    git clone --recurse-submodules git@github.com:project-chip/connectedhomeip.git
    cd connectedhomeip
    git pull
    git submodule update --init

    存储库体积较大,克隆过程需要耗费一些时间。

  4. 下载 build_matter_example.sh 脚本,并将其放在 Matter 的根目录中:

    #!/bin/bash
    set -e
    
    # =============================================================================
    # Matter aarch64 Cross-Compilation Build Script (Unified)
    #
    # This script handles all necessary fixes and configurations:
    # - Bluezoo dependency fix for Python 3.10
    # - TI SDK toolchain wrapper creation
    # - Complete Matter build process
    # =============================================================================
    
    if [[ $# -ne 1 ]]; then
      echo "Error: Please enter exactly one example-name as argument"
      echo "Usage: $0 <your_argument>"
      exit 1
    fi
    
    EXAMPLE_NAME="$1"     
    
    # =============================================================================
    # CONFIGURATION - MODIFY THESE VARIABLES FOR YOUR SETUP
    # =============================================================================
    
    # SDK Path
    SDK_PATH="/home/<user>/ti-processor-sdk-linux-am62lxx-evm-11.00.15.05"
    
    # Path to your aarch64 sysroot
    SYSROOT_AARCH64="$SDK_PATH/filesystem/am62lxx-evm/temp"     # TI SDK sysroot
    
    # Toolchain binary prefix (TI SDK uses aarch64-oe-linux)
    TOOLCHAIN_TARGET="aarch64-oe-linux"       # TI SDK compatible target
    
    # Path to your aarch64 cross-compilation toolchain (using TI SDK native toolchain)
    TOOLCHAIN_PREFIX="$SDK_PATH/linux-devkit/sysroots/x86_64-arago-linux/usr/bin/$TOOLCHAIN_TARGET"  # TI SDK toolchain
    
    # Path to connectedhomeip repository (relative to script location)
    REPO_PATH="."                               # CHANGE THIS if different
    
    echo "=== Matter aarch64 Cross-Compilation Build Script (Unified) ==="
    echo "Toolchain: $TOOLCHAIN_TARGET"
    echo "Sysroot: $SYSROOT_AARCH64"
    echo "Example: $EXAMPLE_NAME"
    echo ""
    
    echo "============================================================================="
    echo "STEP 1: FIX BLUEZOO DEPENDENCY ISSUE"
    echo "============================================================================="
    
    REQUIREMENTS_FILE="$REPO_PATH/scripts/tests/requirements.txt"
    if [ -f "$REQUIREMENTS_FILE" ]; then
        # Check if bluezoo is already commented out
        if grep -q "^bluezoo" "$REQUIREMENTS_FILE"; then
            echo "Commenting out bluezoo dependency (requires Python 3.11+)..."
            sed -i 's/^bluezoo/#bluezoo/' "$REQUIREMENTS_FILE"
            echo "✓ Bluezoo dependency commented out"
        else
            echo "✓ Bluezoo dependency already fixed"
        fi
    else
        echo "Warning: Requirements file not found at $REQUIREMENTS_FILE"
    fi
    
    echo "============================================================================="
    echo "STEP 2: VERIFY PATHS AND TOOLCHAIN"
    echo "============================================================================="
    
    # Construct toolchain binary paths
    export CC_AARCH64="$TOOLCHAIN_PREFIX/${TOOLCHAIN_TARGET}-gcc"
    export CXX_AARCH64="$TOOLCHAIN_PREFIX/${TOOLCHAIN_TARGET}-g++"
    export AR_AARCH64="$TOOLCHAIN_PREFIX/${TOOLCHAIN_TARGET}-ar"
    export STRIP_AARCH64="$TOOLCHAIN_PREFIX/${TOOLCHAIN_TARGET}-strip"
    export LD_AARCH64="$TOOLCHAIN_PREFIX/${TOOLCHAIN_TARGET}-ld"
    
    # Add toolchain to PATH for any remaining usage
    export PATH="$TOOLCHAIN_PREFIX:$PATH"
    
    if [ ! -f "$CC_AARCH64" ]; then
        echo "Error: Compiler not found at $CC_AARCH64"
        echo "Please check your TOOLCHAIN_PREFIX and TOOLCHAIN_TARGET variables"
        exit 1
    fi
    
    if [ ! -d "$SYSROOT_AARCH64" ]; then
        echo "Error: Sysroot not found at $SYSROOT_AARCH64"
        echo "Please check your SYSROOT_AARCH64 path"
        exit 1
    fi
    
    if [ ! -d "$REPO_PATH" ]; then
        echo "Error: Repository not found at $REPO_PATH"
        echo "Please check your REPO_PATH variable"
        exit 1
    fi
    
    echo "✓ Toolchain: $($CC_AARCH64 --version | head -1)"
    echo "✓ Sysroot: $SYSROOT_AARCH64"
    echo "✓ Repository: $REPO_PATH"
    
    echo "============================================================================="
    echo "STEP 3: CREATE TOOLCHAIN WRAPPER"
    echo "============================================================================="
    
    cd "$REPO_PATH"
    # 
    # # Create toolchain wrapper directory
    WRAPPER_DIR="$PWD/toolchain-wrapper-bin"
    mkdir -p "$WRAPPER_DIR"
    
    # Create symbolic links with the names GN expects
    echo "Creating symbolic links for GN compatibility..."
    ln -sf "$TOOLCHAIN_PREFIX/${TOOLCHAIN_TARGET}-gcc" "$WRAPPER_DIR/aarch64-linux-gnu-gcc"
    ln -sf "$TOOLCHAIN_PREFIX/${TOOLCHAIN_TARGET}-g++" "$WRAPPER_DIR/aarch64-linux-gnu-g++"
    ln -sf "$TOOLCHAIN_PREFIX/${TOOLCHAIN_TARGET}-ar" "$WRAPPER_DIR/aarch64-linux-gnu-ar"
    ln -sf "$TOOLCHAIN_PREFIX/${TOOLCHAIN_TARGET}-strip" "$WRAPPER_DIR/aarch64-linux-gnu-strip"
    ln -sf "$TOOLCHAIN_PREFIX/${TOOLCHAIN_TARGET}-ld" "$WRAPPER_DIR/aarch64-linux-gnu-ld"
    ln -sf "$TOOLCHAIN_PREFIX/${TOOLCHAIN_TARGET}-objdump" "$WRAPPER_DIR/aarch64-linux-gnu-objdump"
    ln -sf "$TOOLCHAIN_PREFIX/${TOOLCHAIN_TARGET}-nm" "$WRAPPER_DIR/aarch64-linux-gnu-nm"
    
    echo "✓ Created toolchain wrapper directory: $WRAPPER_DIR"
    echo "Contents:"
    ls -la "$WRAPPER_DIR/"
    
    # Add wrapper to PATH
    export PATH="$PWD/toolchain-wrapper-bin:$PATH"
    
    echo "============================================================================="
    echo "STEP 4: SETUP BUILD ENVIRONMENT"
    echo "============================================================================="
    
    source scripts/activate.sh
    
    echo "Testing cross-compilation..."
    echo 'int main(){return 0;}' > test.c
    $CC_AARCH64 --sysroot="$SYSROOT_AARCH64" -o test test.c
    file test
    rm test test.c
    echo "✓ Cross-compilation test passed"
    
    echo "============================================================================="
    echo "STEP 5: CONFIGURE AND BUILD"
    echo "============================================================================="
    
    #Check if the example exists
    if [ ! -d "examples/${EXAMPLE_NAME}" ]; then
        echo -e "No such '$EXAMPLE_NAME' exists in examples!! \nExiting !!"
        exit 1
    #Check if example does not need specific platform like linux to build
    elif [[ $(find ./examples/ -maxdepth 2 -type f -name args.gni | grep -c "$EXAMPLE_NAME") -gt 0 ]]; then
        ROOT_PATH="examples/$EXAMPLE_NAME"
    #Check if example needs specific platform to build and linux platform is available
    elif [[ $(find ./examples/ -type f -name "args.gni" -path "*/linux/*" | grep -c "$EXAMPLE_NAME") -gt 0 ]]; then
        ROOT_PATH="examples/$EXAMPLE_NAME/linux"
    #Check if example needs specific platform to build but linux platform is NOT available
    else
        echo -e "'$EXAMPLE_NAME' is not supported on Linux!! \nExiting !!"
        exit 1
    fi
    
    gn gen "out/${EXAMPLE_NAME}-arm64" --root="$ROOT_PATH" --args="
      target_cpu=\"arm64\"
      target_os=\"linux\"
      sysroot=\"$SYSROOT_AARCH64\"
      is_clang=false
      treat_warnings_as_errors=false
      target_cflags = [
        \"-D_GNU_SOURCE\", 
        \"-D__USE_GNU\", 
        \"-pthread\",
        \"-DCHIP_DEVICE_CONFIG_WIFI_STATION_IF_NAME=\\\"wlan0\\\"\",
        \"-DCHIP_DEVICE_CONFIG_LINUX_DHCPC_CMD=\\\"udhcpc -b -i %s \\\"\",
      ]
      target_ldflags=[\"-pthread\"]
    "
    
    echo "Building $EXAMPLE_NAME..."
    ninja -C "out/${EXAMPLE_NAME}-arm64"
    
    echo "============================================================================="
    echo "STEP 6: VERIFY BUILD RESULTS"
    echo "============================================================================="
    EXECUTABLE_NAME=$(awk -F'"' '/executable\("/ {print $2}' $ROOT_PATH/BUILD.gn)
    echo "Expected executable name: $EXECUTABLE_NAME"
    BINARY_PATH="out/${EXAMPLE_NAME}-arm64/${EXECUTABLE_NAME}"
    if [ -f "$BINARY_PATH" ]; then
        file "$BINARY_PATH"
        echo "✓ Build complete! Binary located at: $BINARY_PATH"
    else
        echo "Error: Build failed, binary not found at $BINARY_PATH"
        exit 1
    fi
    
    echo "============================================================================="
    echo "BUILD SUMMARY"
    echo "============================================================================="
    echo "Target: aarch64 (ARM64)"
    echo "Toolchain: $TOOLCHAIN_TARGET"
    echo "Example: $EXAMPLE_NAME"
    echo "Output: out/${EXAMPLE_NAME}-arm64/${EXECUTABLE_NAME}"
    echo ""
    echo "All fixes applied:"
    echo "✓ Bluezoo dependency commented out for Python 3.10 compatibility"
    echo "✓ TI SDK native toolchain configured for compatibility"
    echo "✓ Toolchain wrapper created for GN naming conventions"
    echo "✓ Matter build completed successfully"
    echo ""
    echo "To modify configuration, edit the variables at the top of this script:"
    echo "- TOOLCHAIN_PREFIX: $TOOLCHAIN_PREFIX"
    echo "- SYSROOT_AARCH64: $SYSROOT_AARCH64"
    echo "- TOOLCHAIN_TARGET: $TOOLCHAIN_TARGET"
    echo "- EXAMPLE_NAME: $EXAMPLE_NAME"
    echo ""
    echo "To build a different example, run the script with other example's name as argument."
  5. 修改 build_matter_example.sh,以更新以下变量:

    1. SDK_PATH -> 安装的处理器 SDK 的路径。

    2. SYSROOT_AARCH64 -> 处理器 SDK 中提取的文件系统的路径。

  6. 使用以下命令运行脚本:

    # sudo ./build_matter_example.sh <example-name>
    # For example:
    sudo ./build_matter_example.sh chip-tool
    sudo ./build_matter_example.sh lock-app
  7. 注意:在运行上述脚本时,如果您卡在“第 4 步: 设置构建环境”,或您的环境已过时,请退出脚本并运行以下命令:

    sudo -E bash scripts/bootstrap.sh

    这会从头开始重新创建环境,并将耗费一些时间。再次运行 build_matter_example.sh。

  8. 成功构建后,脚本将提及输出二进制文件的路径:<Matter root>/out/<example_directory>/<example_executable>。

  9. 将可执行文件复制到目标。在示例中,我们复制了 'chip-lock-app'(在 AM62L 上)和 'chip-tool'(在 AM62P 上),两个器件连接了相同的网络。

本应用手册中的实验,在最新版本修订时已通过以下 SDK/存储库版本的测试验证:

    处理器 SDK

    11.00.15.05

    Matter 存储库

    提交:e156205783(主分支)