SWAU085F July   2011  – January 2022

 

  1.   Trademarks
  2.   Revision History
  3. 1Requirements
    1. 1.1 System Requirements
    2. 1.2 Configuration Requirements
  4. 2Installation
  5. 3Modes of Operation
    1. 3.1 Serial Port Mode
    2. 3.2 USB Over Android Debug Bridge (ADB) Mode
    3. 3.3 Operational Mode
  6. 4Connection and Firmware Download
    1. 4.1 Register Reads and Writes
    2. 4.2 Power Mode Menu
      1. 4.2.1 Awake Mode
      2. 4.2.2 Listen Mode
      3. 4.2.3 ELP Mode
      4. 4.2.4 Gating Mode
    3. 4.3 Antenna Mode Menu
      1. 4.3.1 Supported Antenna Configuration
      2. 4.3.2 5-GHz Diversity (WL1837MOD and WL1807MOD Only)
  7. 5RX Tab
    1. 5.1 RX Statistics Area
    2. 5.2 Sensitivity Measurements
      1. 5.2.1 Sensitivity Testing Procedure
  8. 6TX Tab
    1. 6.1 TX Packets Section
    2. 6.2 TX Tab Overall Output Power Area
    3. 6.3 TX Tab Tones Area
    4. 6.4 TX Duty Cycle Configuration
    5. 6.5 Output Power Test on the WiLink 8 Device
      1. 6.5.1 TX Testing Procedure
  9. 7Terms and Abbreviations

TX Testing Procedure

To test the output power on the WiLink 8 device, perform the following steps (see Figure 6-5):

  1. In the Overall Output Power area, select dBm mode.
  2. Click the SoC Limits box to enable the SoC limits option.
  3. Using the slider, select a power setting of 30 dBm (see Figure 6-5).
  4. In the Packets area, select the appropriate values from the Rate, Size, and Delay menus.
  5. In the Channel area, set the channel to perform full RF calibration before TX.
  6. To transmit, click the Start TX Packet (Cont.) button.
GUID-3277DFE1-2EFA-4AC2-8001-70D542176DD1-low.png Figure 6-5 WLAN 18xx FW Tab