SWAU085F July   2011  – January 2022

 

  1.   Trademarks
  2.   Revision History
  3. 1Requirements
    1. 1.1 System Requirements
    2. 1.2 Configuration Requirements
  4. 2Installation
  5. 3Modes of Operation
    1. 3.1 Serial Port Mode
    2. 3.2 USB Over Android Debug Bridge (ADB) Mode
    3. 3.3 Operational Mode
  6. 4Connection and Firmware Download
    1. 4.1 Register Reads and Writes
    2. 4.2 Power Mode Menu
      1. 4.2.1 Awake Mode
      2. 4.2.2 Listen Mode
      3. 4.2.3 ELP Mode
      4. 4.2.4 Gating Mode
    3. 4.3 Antenna Mode Menu
      1. 4.3.1 Supported Antenna Configuration
      2. 4.3.2 5-GHz Diversity (WL1837MOD and WL1807MOD Only)
  7. 5RX Tab
    1. 5.1 RX Statistics Area
    2. 5.2 Sensitivity Measurements
      1. 5.2.1 Sensitivity Testing Procedure
  8. 6TX Tab
    1. 6.1 TX Packets Section
    2. 6.2 TX Tab Overall Output Power Area
    3. 6.3 TX Tab Tones Area
    4. 6.4 TX Duty Cycle Configuration
    5. 6.5 Output Power Test on the WiLink 8 Device
      1. 6.5.1 TX Testing Procedure
  9. 7Terms and Abbreviations

Sensitivity Testing Procedure

To measure sensitivity, perform the following steps:

  1. In the Control area of the WLAN 18xx FW RX tab, configure the device to Operational Mode.
  2. In the Channel area, select the channel.
  3. In the Control area of the WLAN 18xx FW RX tab, configure the device to Statistics Mode.
  4. To clear the statistics from the device, click the Reset Statistics button.
  5. Transmit the packets burst from the ESG.
  6. Read the results (statistics) from the device.

Figure 5-2 shows the WLAN 18xx FW RX tab.

GUID-A09B51D0-4B95-41F3-9373-E63C40A33C1B-low.png Figure 5-2 RX GUI