SWAU085F July 2011 – January 2022
Figure 4-6 shows the Power Mode (via MAC) area, which contains the Select menu for the WLAN SoC. The Select menu lists the following power mode options:
TX can be set in awake mode only (for more information on TX, see Figure 4-6, TX Tab).
Figure 4-6 Power Mode Menu