SPRUIY4B February 2023 – May 2024 TMS320F2800152-Q1 , TMS320F2800153-Q1 , TMS320F2800154-Q1 , TMS320F2800155 , TMS320F2800155-Q1 , TMS320F2800156-Q1 , TMS320F2800157 , TMS320F2800157-Q1
Table 5-15explains how the bit field values from the user configurable DCSM OTP location, Z1-OTP-BOOT-GPREG2 or Z2-OTP-BOOT-GPREG2, are decoded by boot ROM.
| Bit | Name | Description | Boot ROM Action |
|---|---|---|---|
| 31:24 | Key | Write 0x5A to indicate to the boot ROM code that the bits in this register are valid. | If user sets to 0x5A, boot ROM uses the values in this register. If set to any other value, boot ROM ignores values in this register. |
| 23:8 | Reserved | Reserved | No Action |
| 7:6 | MPOST(1) | 0x0 = Run MPOST with PLL disabled (10MHz internal oscillator) | When configured to a valid value, MPOST POR memory self-test runs on all device memories |
| 0x1 = Run MPOST with PLL enabled for 115MHz | |||
| 0x2 = Run MPOST with PLL enabled for 57.5MHz | |||
| 0x3 = Disable MPOST | |||
| 5:4 | ERROR_ STS_PIN config |
0x0 – GPIO24, MUX Option 13 | This indicates which GPIO pin is supposed to be used as ERROR_PIN and boot ROM configures the mux as such for the said pin. The ERROR_STS pin mux configuration is locked by the boot ROM, but not committed. |
| 0x1 – GPIO28, MUX Option 13 | |||
| 0x2 – GPIO29, MUX Option 13 | |||
| 0x3 – ERROR_STS function disabled (default) | |||
| 3:0 | CJTAGNODEID | CJTAGNODEID[3:0] | Boot ROM takes this values and programs the lower 4 bits of the CJTAGNODEID register. |