SPRUIY4B February 2023 – May 2024 TMS320F2800152-Q1 , TMS320F2800153-Q1 , TMS320F2800154-Q1 , TMS320F2800155 , TMS320F2800155-Q1 , TMS320F2800156-Q1 , TMS320F2800157 , TMS320F2800157-Q1
This sections gives details about the entry point addresses for various boot modes. These entry points direct the boot ROM what address to branch to at the end of booting as per the selected boot mode.
Table 5-16 gives details about the entry point addresses for Flash boot mode.
Table 5-17 gives details about the entry point addresses for RAM boot mode.
Table 5-18 gives details about the entry point addresses for Secure Flash boot mode.
| Option | BOOTDEFx Value | Flash Sector | Address | Packages Supported |
|---|---|---|---|---|
| 0 | 0x03 | CPU Bank 0 Sector 0 | 0x0008 0000 | All |
| 1 | 0x23 | CPU Bank 0 Sector 32 | 0x0008 8000 | All |
| 2 | 0x43 | CPU Bank 0 End of Sector 63 | 0x0008 FFF0 | All |
| 3 | 0x63 | CPU Bank 0 Sector 64 | 0x0009 0000 | All |
| 4 | 0x83 | CPU Bank 0 End of Sector 96 | 0x0009 8000 | All |
| 5 | 0xA3 | CPU Bank 0 End of Sector 127 | 0x0009 FFF0 | All |
| Option | BOOTDEFx Value | RAM Entry Point | Package Supported |
|---|---|---|---|
| 0 | 0x05 | 0x0000 0000 | All |
| Option | BOOTDEFx Value | Flash Sector | Address | Packages Supported |
|---|---|---|---|---|
| 0 (default) | 0x0A | CPU Bank 0 Sector 0 | 0x0008 0000 | All |
| 1 | 0x2A | CPU Bank 0 Sector 32 | 0x0008 8000 | All |
| 2 | 0x4A | CPU Bank 0 End of Sector 63 | 0x0008 FFF0 | All |
| 3 | 0x6A | CPU Bank 0 Sector 64 | 0x0009 0000 | All |
| 4 | 0x8A | CPU Bank 0 End of Sector 96 | 0x0009 8000 | All |