SPRUI33H November 2015 – June 2024 TMS320F280040-Q1 , TMS320F280040C-Q1 , TMS320F280041 , TMS320F280041-Q1 , TMS320F280041C , TMS320F280041C-Q1 , TMS320F280045 , TMS320F280048-Q1 , TMS320F280048C-Q1 , TMS320F280049 , TMS320F280049-Q1 , TMS320F280049C , TMS320F280049C-Q1
Table 11-10 lists the memory-mapped registers for the ERAD_HWBP_REGS registers. All register offset addresses not listed in Table 11-10 should be considered as reserved locations and the register contents should not be modified.
| Offset | Acronym | Register Name | Write Protection | Section |
|---|---|---|---|---|
| 0h | HWBP_MASK | HWBP (EBC) Mask Register | EALLOW | Go |
| 2h | HWBP_REF | HWBP (EBC) Reference Register | EALLOW | Go |
| 4h | HWBP_CLEAR | HWBP (EBC) Clear Register | EALLOW | Go |
| 6h | HWBP_CNTL | HWBP (EBC) Control Register | EALLOW | Go |
| 7h | HWBP_STATUS | HWBP (EBC) Status Register | EALLOW | Go |
Complex bit access types are encoded to fit into small table cells. Table 11-11 shows the codes that are used for access types in this section.
| Access Type | Code | Description |
|---|---|---|
| Read Type | ||
| R | R | Read |
| R-0 | R -0 | Read Returns 0s |
| Write Type | ||
| W | W | Write |
| Reset or Default Value | ||
| -n | Value after reset or the default value | |
HWBP_MASK is shown in Figure 11-8 and described in Table 11-12.
Return to the Summary Table.
HWBP (EBC) Mask Register
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| MASK | |||||||||||||||||||||||||||||||
| R/W-0h | |||||||||||||||||||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-0 | MASK | R/W | 0h | This register contains address mask for comparison. The contents of this register are used along with the reference register to determine the address match. The equation used to determine a match is as follows. Match is true if, (address | mask) == (ref | mask) This register is writable by CPU only if application owns the unit and if EALLOW is set. Otherwise, the writes are ignored. The register is writable by the debugger only if the debugger owns this unit. Otherwise, the writes are ignored. Reset type: ERAD_RESET |
HWBP_REF is shown in Figure 11-9 and described in Table 11-13.
Return to the Summary Table.
HWBP (EBC) Reference Register
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| REF | |||||||||||||||||||||||||||||||
| R/W-0h | |||||||||||||||||||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-0 | REF | R/W | 0h | This register contains the reference address for comparison. The contents of this register are used along with the mask register to determine the address match. The equation used to determine a match is as follows. Match is true if, (address | mask) == (ref | mask) This register is writable by CPU only if application owns the unit and if EALLOW is set. Otherwise, the writes are ignored. The register is writable by the debugger only if the debugger owns this unit. Otherwise, the writes are ignored. Reset type: ERAD_RESET |
HWBP_CLEAR is shown in Figure 11-10 and described in Table 11-14.
Return to the Summary Table.
HWBP (EBC) Clear Register
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | |||||||
| R-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | EVENT_CLR | ||||||
| R-0h | R-0/W-0h | ||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 15-1 | RESERVED | R | 0h | Reserved |
| 0 | EVENT_CLR | R-0/W | 0h | Event Clear register: 0 No action. 1 A write with this bit set to 1 will clear the sticky EVENT_FIRED bit in the HWBP_STATUS register and bring the Breakpoint Module statemachine status back to IDLE. Reads of this bit position will always return a 0. Reset type: ERAD_RESET |
HWBP_CNTL is shown in Figure 11-11 and described in Table 11-15.
Return to the Summary Table.
HWBP (EBC) Control Register
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | RESERVED | RESERVED | COMP_MODE | ||||
| R-0h | R/W-0h | R-0h | R/W-0h | ||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| COMP_MODE | RTOSINT | STOP | BUS_SEL | RESERVED | |||
| R/W-0h | R/W-0h | R/W-0h | R/W-0h | R-0h | |||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 15-12 | RESERVED | R | 0h | Reserved |
| 11 | RESERVED | R/W | 0h | Reserved |
| 10 | RESERVED | R | 0h | Reserved |
| 9-7 | COMP_MODE | R/W | 0h | Enhanced Bus Comparator (EBC) compare modes: 000 Regular masked compare HWBP_MSK will be ignored for the following modes: 100 Bus value GT HWBP_REF 101 Bus value GE HWBP_REF 110 Bus value LT HWBP_REF 111 Bus value LE HWBP_REF GT means Greater Than GE means Greater or Equal LT means Less Than LE means Lesser or Equal Reset type: ERAD_RESET |
| 6 | RTOSINT | R/W | 0h | This bit decides whether the Enhanced Bus Comparator (EBC) unit will generate RTOSINTn interrupt when event matches occur. Note that the event outputs will always be generated regardless of the state of this bit. 0 The Enhanced Bus Comparator (EBC) unit will not cause any action towards the CPU. 1 The Enhanced Bus Comparator (EBC) unit will assert RTOSINTn for matching data accesses and trace tags for matching program fetches. Reset type: ERAD_RESET |
| 5 | STOP | R/W | 0h | This bit decides whether the Enhanced Bus Comparator (EBC) unit will generate CPU halting signals when event matches occur. Note that the event outputs will always be generated regardless of the state of this bit. 0 The Enhanced Bus Comparator (EBC) unit will not cause any action towards halting the CPU. 1 The Enhanced Bus Comparator (EBC) unit will assert ANASTOP for matching data accesses and break tags for matching program fetches. These can cause the CPU to HALT Reset type: ERAD_RESET |
| 4-2 | BUS_SEL | R/W | 0h | These bits are used to select which CPU buses will be used for comparison to generate the match events. For each bus selected, the corresponding strobes will automatically be selected to determine valid accesses. 000 PAB for instruction fetches 011 DRAB for data read accesses 010 DWAB for data write accesses 001 VPC for Program counter match 100 DWDB for write data match All other combinations are RESERVED. Reset type: ERAD_RESET |
| 1-0 | RESERVED | R | 0h | Reserved |
HWBP_STATUS is shown in Figure 11-12 and described in Table 11-16.
Return to the Summary Table.
HWBP (EBC) Status Register
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| STATUS | MODULE_ID | ||||||
| R-0h | R-4h | ||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | EVENT_FIRED | ||||||
| R-0h | R-0h | ||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 15-14 | STATUS | R | 0h | Bus comaparator status: 00 Idle 10 Enabled 11 Completed Reset type: ERAD_RESET |
| 13-8 | MODULE_ID | R | 4h | These bits are always a constant representing a unique identification for the Enhanced Bus Comparator (EBC) unit. Reset type: ERAD_RESET |
| 7-1 | RESERVED | R | 0h | Reserved |
| 0 | EVENT_FIRED | R | 0h | This is a sticky bit which gets set every time the HWBP (EBC) unit generates a match event. This will be used by software to figure out whether this HWBP module fired an event or not. This bit will get cleared by writing a '1' to bit 0 of the HWBP_CLEAR register. Reset type: ERAD_RESET |