SPRUHM8K December 2013 – May 2024 F28377D-SEP , TMS320F28374D , TMS320F28375D , TMS320F28376D , TMS320F28377D , TMS320F28377D-EP , TMS320F28377D-Q1 , TMS320F28378D , TMS320F28379D , TMS320F28379D-Q1
Each CPU has a non-maskable interrupt (NMI) module that detects hardware errors in the system. Each NMI module has a watchdog timer that triggers a reset, if the CPU does not respond to an error within a user-specified amount of time. The CPU1 NMI watchdog reset (CPU1.NMIWDRS) produces an XRS. The CPU2 NMI watchdog reset (CPU2.NMIWDRS) produces a CPU2.SYSRS and triggers an NMI on CPU1.
After an NMI watchdog reset, the NMIWDRSn bit in RESC is set.