SPRUHM8K December 2013 – May 2024
So far, none of the examples have made use of the phase register (TBPHS). It has either been set to zero or a don't care. However, by programming appropriate values into TBPHS, multiple PWM modules can address another class of power topologies that rely on phase relationship between legs (or stages) for correct operation. As described in the time-base submodule section, a PWM module can be configured to allow a SyncIn pulse to cause the TBPHS register to be loaded into the TBCTR register. To illustrate this concept, Figure 15-69 shows a master and slave module with a phase relationship of 120° (that is, the slave leads the master).
Figure 15-69 Configuring Two PWM Modules for Phase Control
Figure 15-70 shows the associated timing waveforms for this configuration. Here, TBPRD = 600 for both master and slave. For the slave, TBPHS = 200 (that is, 200/600 x 360° = 120°). Whenever the master generates a SyncIn pulse (CTR = PRD), the value of TBPHS = 200 is loaded into the slave TBCTR register so the slave time-base is always leading the master time-base by 120°.
Figure 15-70 Timing Waveforms Associated with Phase Control Between Two Modules