SPRADS1 June 2025 F29H850TU
The FOTA_Example_Application project is a modified LED blinky example that is able to leverage the flash-based SBL project. The main capability that allows this application to be compatible with the flash-based SBL is the ability to branch to receive commands from the host programmer and branch to the appropriate region of the SBL. In the following section, this document describes how that is achieved.