SPRACU9 October   2021 F29H850TU , F29H859TU-Q1 , F29P329SM-Q1 , TMS320F2800152-Q1 , TMS320F2800153-Q1 , TMS320F2800154-Q1 , TMS320F2800155 , TMS320F2800155-Q1 , TMS320F2800156-Q1 , TMS320F2800157 , TMS320F2800157-Q1 , TMS320F280033 , TMS320F280034 , TMS320F280034-Q1 , TMS320F280036-Q1 , TMS320F280036C-Q1 , TMS320F280037 , TMS320F280037-Q1 , TMS320F280037C , TMS320F280037C-Q1 , TMS320F280038-Q1 , TMS320F280038C-Q1 , TMS320F280039 , TMS320F280039-Q1 , TMS320F280039C , TMS320F280039C-Q1 , TMS320F28384D , TMS320F28384D-Q1 , TMS320F28384S , TMS320F28384S-Q1 , TMS320F28386D , TMS320F28386D-Q1 , TMS320F28386S , TMS320F28386S-Q1 , TMS320F28388D , TMS320F28388S , TMS320F28P550SG , TMS320F28P550SJ , TMS320F28P559SG-Q1 , TMS320F28P559SJ-Q1 , TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1

 

  1.   Trademarks
  2. 1Introduction
    1. 1.1 MCAN Features
  3. 2Useful tips to run the C2000ware examples
  4. 3Program Descriptions
  5. 4Debug and Design Tips to Resolve/Avoid CAN Communication Issues
    1. 4.1 Minimum Number of Nodes Required
    2. 4.2 Why a Transceiver is Needed
    3. 4.3 Debug Checklist
      1. 4.3.1 Programming Issues
      2. 4.3.2 Physical Layer Issues
      3. 4.3.3 Hardware Debug Tips
  6. 5How to Duplicate (clone) an Existing Project
  7. 6How to Get Visibility Into Driverlib Files
  8. 7References

Physical Layer Issues

  • Has the bus been terminated correctly (with 120-Ω) at either ends (only)? The bus must be terminated only at either ends and with a 120-Ω resistor. In other words, no more than two terminator resistors may be present on the bus, unless split termination is followed, in which case there will be two resistors on either ends. While designing a CAN bus system, it is important that the termination resistors can be enabled/disabled from outside the system enclosure. This scheme makes it easy when nodes have to be added or removed to/from the network.
  • Are all CAN nodes configured for the same bit-rate? Mis-matched node bit rates would repeatedly introduce error frames on the bus. Capture the output of the CANTX pin on the oscilloscope to physically verify the bit-time.
  • Have you tried a lower bit-rate? Say, 50 kbps, for example? Timing issues concerning propagation delays may be caught trying a lower bit-rate. Ensure that the NBTP and DBTP registers have the programmed value.
  • Have you tried to reduce the bus length and number of nodes?
  • Before the occurrence of the error condition, were any error-frames seen on the bus? This could point to timing violations or noise issues.
  • How many nodes are there in the bus? (In non-self-test mode, there must be at least two nodes on the network, due to the acknowledge (ACK) requirement mandated by the CAN protocol).