SPRACH9E November   2021  – February 2024 AWR1443 , AWR1642 , AWR1843 , AWR2544 , AWR2944 , AWR6843 , AWR6843AOP , IWR1443 , IWR1642 , IWR1843 , IWR6443 , IWR6843 , IWR6843AOP

 

  1.   1
  2.   Flash Variants Supported by the mmWave Sensor
  3.   Trademarks
  4. 1Introduction
  5. 2Serial Data FLASH Supported
    1. 2.1 AWR1243/xWR1443 ES1.0 and ES2.0 Devices
    2. 2.2 AWR294x, AWR2544, xWR1642, xWR1843, xWR6843 Devices and AWR1243/xWR1443 ES3.0 Devices
      1. 2.2.1 Prerequisite
      2. 2.2.2 ROM-Assisted Download to the FLASH (Device Management Mode - SOP5)
      3. 2.2.3 ROM-Based Load From FLASH (Functional Mode – SOP4)
      4. 2.2.4 Recommendation
    3. 2.3 Known Issues (xWR1642 ES1.0 and xWR6843 ES1.0 Devices)
    4. 2.4 Flash Variants
      1. 2.4.1 Flash Variants
  6. 3Revision History

Known Issues (xWR1642 ES1.0 and xWR6843 ES1.0 Devices)

The ROM bootloader in XWR1642 pre-production devices is not compatible with SFLASH variants that support extended addressing mode. In particular, the “Number of Address length” field of the SFDP command response being non-zero is not supported. The total SFLASH addressable region in XWR1642 devices is 8 MBytes. Thus, “Number of Address length” = 0 (corresponding to 3 bytes address length) satisfies the addressable range. However, the compatibility issue is with variants that allow for 3 or 4 bytes address length.

This incompatibility will be addressed in the production version of the XWR1642 silicon.