SNLU254A November   2020  – July 2022 DS160PT801

 

  1.   Abstract
  2.   Trademarks
  3. 1EVM Control and Configuration Information
    1. 1.1 Retimer Pin Controls
    2. 1.2 USB-to-SMBus Interface
    3. 1.3 PCIe PRSNT# Signal Control and Configuration
    4. 1.4 PCIe Reference Clock Control and Configuration
  4. 2EVM Power
    1. 2.1 EVM Current Sensing
  5. 3SigCon Architect GUI
    1. 3.1 Setup and Installation
    2. 3.2 Configuration Page
    3. 3.3 Low-Level Page
    4. 3.4 EEPROM Page
    5. 3.5 Control Panel
    6. 3.6 High-Level Page
    7. 3.7 Diagnostic Page
    8. 3.8 Eye Monitor Page
  6. 4PCB Material Information
    1. 4.1 DS160PT801 PCB Design
    2. 4.2 DS160PT801 PCB Stackup
    3. 4.3 DS160PT801 PCB Power Distribution
    4. 4.4 DS160PT801 Local Decoupling
  7. 5DS160PT801X16EVM Schematic
  8. 6Hardware BOM
  9. 7Revision History

Low-Level Page

GUID-20220603-SS0I-J4BJ-QLPS-8HMJXCVCXFDL-low.png Figure 3-2 Low-Level Page Screenshot

The Low-Level page of the GUI is used for basic register access to the register map of the DS160PT801 retimer by providing SMBus read and write functions. The ability to save a specific retimer configuration for use later is also provided and can be used performing system evaluation. The description of the input fields of the Low-Level page are as follows.

  • Device Select Dropdown allows a user to change the active register map from either the link-width manager or link-width follower SMBus address.
  • Block Select Dropdown allows a user to change the active register block between Global, Shared, Channel, or PLL registers.
  • Current Address Field displays the currently selected register address.
  • Data Field displays the data currently stored at the selected register address.
  • Mask Value Field displays the mask value that will be used for write operations at this register. Only the bits that are set to a "1" in this field will be written to.
  • Write Register Button issues an SMBus write of the data listed in the data field at the current address using the bit mask indicated in the Mask Value field.
  • Broadcast Button becomes active when one of the channel register blocks are selected. Clicking this button performs a write operation similar to the Write Register button, but it will broadcast the write to all channels in the currently selected device.
  • Read Register Button issues an SMBus read of the data listed in the current address field.
  • Read All Button issues a SMBus read of all registers for the currently selected register block.
  • Reset Device Button resets all register values back to their default values. This will cause an active PCIe link to fail.
  • Load Config Button can be used to load a previously saved set of SMBus register values.
  • Save Config Button saves a file that stores the current values for all SBMus registers. This file can later be loaded using the Load Config button.