SNAU252 June 2020
The SYNC / SYSREF page allows some mode set buttons for JESD204B features. The SYNC dividers button will stop all SYNC inputs, set normal SYNC mode, enable all dividers for SYNC, issue a SYNC by toggling SYNC_POL, set all dividers to ignore SYNC, then return any other changed parameter to its original state. This is a nice feature to ensure all outputs are synchronized together or to be run after changing the digital delay value which requires a SYNC to update. This functionality is also available on any other page through the toolbar as SYNC Dividers.
NOTE
To use SYNC or SYSREF, ensure that SYNC_EN = 1. To use SYSREF in continuous, pulser, or reclocked modes, be sure SYSREF_PD = 0.
The SCLKX_Y_DIS_MODE bits allow the clock outputs to be disabled or set to a low state. Because values 1 and 2 are only conditionally set by the SYSREF_GBL_PD bit, it is possible to power up or power down several SYSREF outputs by programming only one register. When changing between 0x00 (Active) and (0x01) Conditional Low, keeping the SYSREF_CLR = 1 during transition will prevent glitch pulses from the SYSREF output.
Figure 20. TICS Pro - SYNC / SYSREF Page