SLVAFX0B October 2024 – March 2026 TLV702 , TLV703 , TLV755P , TPS74401 , TPS7A13 , TPS7A14 , TPS7A20 , TPS7A21 , TPS7A49 , TPS7A52 , TPS7A53 , TPS7A53B , TPS7A54 , TPS7A57 , TPS7A74 , TPS7A83A , TPS7A84A , TPS7A85A , TPS7A91 , TPS7A92 , TPS7A94 , TPS7A96 , TPS7H1111-SP
The NR/SS filter significantly improves the power supply rejection ratio (PSRR) and noise in LDO regulators [21].
The time constant for the NR/SS filter can result in longer than desired turn-on times for some applications. Modern LDO regulators can include a fast charge circuit to reduce the turn-on time of the filtered reference supply, and by extension, the output voltage. The fast-charge circuit operates while VNR/SS measures less than the changeover voltage (VCO), when the steady state filter values are used.
Figure 2-5 shows typical turn-on behavior of an LDO regulator using fast charge.
For LDO regulators that use a voltage reference, this fast-charge circuit is either a parallel resistor or parallel current source with the NR/SS resistor as shown in Figure 2-1. For LDO regulators that use a current reference, the fast-charge circuit modifies the IREF current to be a larger value as shown in Figure 2-2. Equation 11 calculates the time when the changeover voltage occurs (tCO). Entering = tCO into Equation 7 yields the initial condition (VCO_FF) on VTOP just after the changeover voltage event.
If a fast-charge current source is across RNR/SS, use Equation 12 instead of Equation 11 to calculate tCO.
Equation 11. Equation 12. |
Common values of VCO are 95% to 97% of VREF. Use Equation 5 or Equation 6 to calculate VFB(t) during fast-charge operation, but after the fast-charge function completes, use Equation 13.
If the LDO uses a precision current source, (as shown in Figure 2-2) use Equation 14.
Use Equation 15 to calculate VTOP after the changeover event. Equation 13 defines VFB(t).