SLUUCO9B April 2023 – December 2025 BQ28Z620
The BQ28Z620 is required to be in RELAX mode before it can check if the cells are unbalanced and how much balancing is required. The BQ28Z620 enters RELAX mode when:
Current() < Quit Current for at least Dsg Relax Time when coming from DISCHARGE mode for Chg Relax Time when coming for CHARGE mode.
Figure 9-1 Entering CHARGE or RELAX ModeOnce in RELAX mode, the BQ28Z620 waits until an OCV measurement is taken, which occurs after:
The determination of when to update the OCV data is part of the normal Impedance Track algorithm and is not specific to the cell balancing algorithm.
Figure 9-2 OCV MeasurementThe BQ28Z620 then calculates the amount of charge difference between cells with a higher state-of-charge than the lowest cell SOC. The value, dQ, is determined for each cell based by converting the measured OCV to Depth-of-Discharge (DOD) percentages using a temperature-compensated DOD vs. OCV table lookup table. If the measured, OCV does not coincide with a specific table entry, then the DOD value is linearly interpolated from the two adjacent DODs of the respective table adjacent OCVs.
The delta in DOD% between each cell and the cell of lowest SOC is multiplied by the respective cells QMax to create dQ: for example, dQ = CellnDOD – CellLOWEST_SOC DOD × CellnQMax (mAh).
Figure 9-3 ΔQ CalculationThe BQ28Z620 calculates the required balancing time using dQ and Bal Time/mAh Cell 1 (for cell 1) or Bal Time/mAh Cell 2. The value of Bal Time/mAh Cell 1 and Bal Time/mAh Cell 2 is fixed based on key system factors and is calculated by:
Cell balancing time for each cell to be balanced is calculated by: dQCelln × Bal Time/mAh Cell 1 for cell1 or and dQCelln × Bal Time/mAh Cell 2. The cell balancing time is stored in the 16-bit RAM register CellnBalanceTimer, providing a maximum calculated time of 65535 s (or 18.2 hrs). This update only occurs if a valid QMax update has been made; otherwise, they are all set to 0.
The CellnBalanceTimer registers are clamped at 0xFFFF and cannot roll over.