SLUUCD5A January 2023 – June 2026 BQ27427
This read-only function returns an unsigned integer value of the internal temperature sensor in units of 0.1 K as measured by the fuel gauge. If OpConfig [TEMPS] = 00, this command will return the same value as Temperature().