SLUUCD5A January 2023 – June 2026 BQ27427
This read- and write-word function returns an unsigned integer value of the temperature in units of 0.1 K measured by the fuel gauge. If OpConfig [TEMPS] bits = 00 (default), a read command will return the internal temperature sensor value and a write command will be ignored. If OpConfig [TEMPS] bits = 01, a read command will return the temperature measured through an external thermistor. If OpConfig [TEMPS] bits = 10, a write command sets the temperature to be used for gauging calculations, while a read command returns to the temperature previously written.