SLUUBT4B June 2018 – June 2025
The EVM is configured to support six LEDs to provide state-of-charge information for the cells. If configured with the correct jumpers, press the LED DISPLAY button to illuminate the LEDs for approximately 4 seconds. Alternately, the LED's can be turned on with in the Commands tab with the LED_TOGGLE to test the LED function, or DISPLAY_PRESS to display the Relative State of Charge.