SLUUBT4B June 2018 – June 2025
The BQ40Z80 data memory comes configured per the default settings detailed in the BQ40Z80 Technical Reference Manual (TRM). Make sure that the settings are correctly changed to match the pack and application for the implementation being evaluated.
The correct setting of these options is essential to get the best performance. The settings can be configured using the Data Memory screen (see Figure 2-3).
Figure 2-3 Data Memory Screen