SLUUBT4B June 2018 – June 2025
This section contains information on modifying the EVM and using various features on the reference design. The jumpers on the board allow different pin configurations. The pin configuration in the registers must match the jumper configuration on the bq40z80EVM . The Pin Configuration register can be set in the Data Memory section of bqStudio. If a register is set to an undefined setting, the output is configured as high-Z.
| General Description | Pin Configuration Register Setting | Jumper Connections | Comments | |
|---|---|---|---|---|
| Pack connector with SYS_PRES | J1 | Connect PACK+ and PACK– to the appropriate pins on the battery pack | ||
| Header for cell connections | J12 | Pin 1: 7P, Pin2: 6P, Pin3: 5P, Pin4: 4P, Pin5: 3P, Pin6: 2P, Pin7: 1P, Pin8: 1N(GND). If using less than 7 cells, tie the unused cell pins (6P, 5P, etc) to the highest cell in the stack | ||
| Pin 12 | V7SENSE | [MFP12_SEL2:MFP12_SEL0]=000 DEFAULT | J20[1,2], J7[1,2] | Connects Pin 12 as V7SENSE to the middle of the voltage divider |
| TS3 | [MFP12_SEL2:MFP12_SEL0]=001 | J20[2,3] | Connects Pin 12 as TS3 to a 10k NTC | |
| ADCIN1 | [MFP12_SEL2:MFP12_SEL0]=010 | J20[1,2], J7[2,3] | Connects Pin 12 to Pin 1 of J11. Connect a voltage between 0V and 1V to have the ADC read the voltage at this pin | |
| GPIO | [MFP12_SEL2:MFP12_SEL0]=011 | J20[1,2], J7[2,3] | Connects Pin 12 to Pin 1 of J11. Use this pin as a GPIO | |
| Pin 13 | /DISP | [MFP13_SEL2:MFP13_SEL0]=000 DEFAULT | J21[1,2], J14[1,2] | Connects Pin 13 (/DISP) to TP5 and S3 |
| TS4 | [MFP13_SEL2:MFP13_SEL0]=001 | J21[2,3] | Connects Pin 12 as TS4 to a 10k NTC | |
| ADCIN2 | [MFP13_SEL2:MFP13_SEL0]=010 | J21[1,2], J14[2,3] | Connects Pin 13 to Pin 5 of J11. Connect a voltage between 0V and 1V to have the ADC read the voltage at this pin | |
| GPIO | [MFP13_SEL2:MFP13_SEL0]=011 | J21[1,2], J14[2,3] | Connects Pin 13 to Pin 5 of J11. Use this pin as a GPIO | |
| Pin 15 | VC7EN | [MFP15_SEL1:MFP15_SEL0]=00 DEFAULT | J6[1,2] | Connects Pin 15 (VC7EN) to the gate of Q6 to enable the voltage divider so a scaled voltage of the top of stack is applied to VC7SENSE |
| /DISP | [MFP15_SEL1:MFP15_SEL0]=01 | J6[2,3], J8[1,2] | Connects Pin 15 (/DISP) to TP5 and S3 | |
| GPIO | [MFP15_SEL1:MFP15_SEL0]=10 | J6[2, 3], J8[2, 3] | Connects Pin 15 (GPIO) to Pin 2 of J11 | |
| Pin 16 | CB7EN | [MFP16_SEL1:MFP16_SEL0]=00 DEFAULT | J10[1,2] | Connects Pin 17 (CB7EN) to the gate of Q11 for external cell balancing for the 7th cell |
| PDSG | [MFP16_SEL1:MFP16_SEL0]=01 | J10[2, 3], J9[1,2] | Connects Pin 16 (PDSG) to the gate of Q7 to enable pre-discharge through Q5 | |
| GPIO | [MFP16_SEL1:MFP16_SEL0]=10 | J10[2,3], J9[2,3] | Connects Pin 62 to Pin 4 of J11. Use this pin as a GPIO | |
| Pin 17 | /PRES | [MFP17_SEL2:MFP17_SEL0]=000 DEFAULT | J5[1,2] | Connects Pin 17 (/PRES) to Pin 3 of J2 |
| SHUTDN | [MFP17_SEL2:MFP17_SEL0]=001 | J5[1,2] | Connects Pin 17 (/SHUTDN) to S3 pushbutton | |
| /DISP | [MFP17_SEL2:MFP17_SEL0]=010 | J5[2,3], J3[1,2] | Connects Pin 17 (/DISP) to TP5 and S2 | |
| PDSG | [MFP17_SEL2:MFP17_SEL0]=011 | J5[2,3], J3[2, 3], J4[1,2] | Connects Pin 17 (PDSG) to the gate of Q7 to enable pre-discharge through Q5 | |
| GPIO | [MFP17_SEL2:MFP17_SEL0]=100 | J5[2,3], J3[2,3], J4[2,3] | Connects Pin 17 (GPIO) to Pin 3 of J11 | |
| Pin 20 | LEDCNTLA | [MFP20_SEL2:MFP20_SEL0]=000 DEFAULT | J15[2,3] | Connects pin 20 to LEDs to be used as LEDCNTLA. Must be used with LEDCNTLB and LEDCNTLC |
| PDSG | [MFP20_SEL2:MFP20_SEL0]=010 | J15[1,2], J13[1,2] | Connects pin 20 (PDSG) to the gate of Q7 to enable pre-discharge through Q5. In this mode, Pins 21 and Pin 22 are used as GPIOs. | |
| GPIO | [MFP20_SEL2:MFP20_SEL0]=001 | J15[1,2], J13[2,3] | Connects Pin 20 to Pin 6 of J11. Use this pin as a GPIO | |
| Pin 21 | LEDCNTLB | [MFP20_SEL2:MFP20_SEL0]=000 DEFAULT | J17[1,2] | Connects pin 21 to LEDs to be used as LEDCNTLB. Must be used with LEDCNTLA and LEDCNTLC |
| GPIO | [MFP20_SEL2:MFP20_SEL0]=010 or [MFP20_SEL2:MFP20_SEL0]=001 | J17[2,3] | Connects Pin 21 to Pin 7 of J11. Use this pin as a GPIO | |
| Pin 22 | LEDCNTLC | [MFP20_SEL2:MFP20_SEL0]=000 DEFAULT | J16[1,2] | Connects pin 22 to LEDs to be used as LEDCNTLC. Must be used with LEDCNTLA and LEDCNTLB |
| GPIO | [MFP20_SEL2:MFP20_SEL0]=010 or [MFP20_SEL2:MFP20_SEL0]=001 | J16[2,3] | Connects Pin 22 to Pin 8 of J11. Use this pin as a GPIO | |