In additional to rectification and inversion, voltage regulation, control of harmonics, reactive power compensation and wave shaping is required for ensuring the HVDC station operates reliably meeting operational requirements and providing the required power output. Some of the equipments connected include:
- Smoothing reactors: It is a coil connected to DC line that reduces ripple and
harmonics in DC link, Limits over current during faults, Prevent current from
being discontinuous for light loads and also helps to prevent from commutation
failure.
- Harmonic filters: Converters generate harmonics in voltages and currents. These
harmonics can cause overheating of capacitors and nearby generators and
interference with telecommunication systems. Harmonic filters are used to
mitigate these harmonics.
- Reactive power supply: Under steady state condition, the reactive power drawn
by the converter is about 10-50% of the active power transferred and is provided
by the shunt capacitor bank.
- Earthing Electrodes: Electrodes are conductors that provide connection to the
earth. They have large surfaces to minimize current densities and surface
voltage gradients.