SLOA289C May 2020 – May 2026 66AK2H06 , 66AK2H12 , 66AK2H14 , ADS8588H , AMC3301 , ISO224 , ISO7740 , ISO7741 , ISO7742 , LMZ30604 , SN65LVDS047 , SN65LVDS048A , UCC12040 , UCC12050
To utilize DC, a conversion step is necessary. In order to convert high voltage AC power to DC power, two technologies are available, classical Line Commutated Converter (LCC) and the Voltage Source Converter (VSC). LCC is commonly called as HVDC Classic, while VSC has a several names, like HVDC Light (ABB), HVDC Plus (Siemens), HVDC MaxSine (Alstom) and Flexible HVDC (China).
LCC converter technology is based on a semiconductor-based switch named thyristor. Thyristors need to be turned on, or fired, to start conducting current. These switches can withstand the AC voltage in either polarity but current can only flow in one direction and can be limited by adjusting the time the thyristors are turned on. This time, or angle in a sinusoid, at which the thyristors are turned on is called the firing angle, or valve ignition delay angle, and is used to control power flow between the HVDC stations.
Voltage Source Converter technology is based on Insular Gate Bipolar Transistors (IGBT). The IGBT can be controlled both with regards to being turned on or off. In VSC technology, the DC current can flow in both directions. That is a benefit over the LCC technology in which the current can flow in one direction. Considering the bi-directional capability of the DC current flow in VSC, there is no need to change the DC voltage polarity of the converters to change the power flow direction between converters. Compared to LCC technology, it is possible for VSC to be connected to weak grids that has low short-circuited level.
In VSC based HVDC, Power can be controlled by changing the phase angle of the converter AC voltage with respect to the filter bus voltage, whereas the reactive power can be controlled by changing the magnitude of the fundamental component of the converter AC voltage with respect to the filter bus voltage. By controlling these two aspects of the converter voltage, operation in all four quadrants is possible.