SLAU330B May 2011 – April 2017
The MSP-EXP430F5529 board is designed specifically to demonstrate the MSP430F5529.
Verify that the jumpers are configured correctly. See Section 4 for jumper configuration.
Verify that the target device is powered properly.
If the target is powered locally, verify that the supplied VCC is sufficient to power the board. Check the device data sheet for the specification.
Improper programming of the device could lead to a JTAG total lockup condition. The cause of this problem might be an incorrect device selection when creating a new project in CCS (select MSP430F5529) or programming the device without a stable power source (low battery, switching the Power Selector while programming, or absence of the MSP430 power jumper JP6 during programming).
To solve this, completely reset the device. First unplug all power sources and connections (JTAG and USB cables). Set the Power Selector Switch to FET mode. Use a jumper cable to briefly short one of the GND test points with the 430 PWR test point. The device should now be released from the lockup state.
No. Fuse blow capability is inherent to all flash-based MSP430 devices to protect user's intellectual property. Care must be taken to avoid the enabling of the fuse blow option during programming, because blowing the fuse would prevent further access to the MSP430 device through JTAG.
The LCD and the LCD backlight require a large amount of current (approximately 20 mA to 25 mA) to operate. This results in a total system current consumption in the range of 30 mA. If the LCD backlight is on, 30 mA is considered normal.
To ensure the board is OK, disable the LCD and the LCD backlight and measure the current again. The entire board current consumption should not exceed 10 mA at this state. Note that the current consumption of the board could vary greatly depending on the optimization of the board configurations and the applications.
The expected current consumption for the MSP430F5529 in standby mode (LPM3), for example, is approximately 2 μA. Operating at 1 MHz, the total current consumption should not exceed approximately 280 μA.
The LCD contrast is highly dependent on the voltage of the system. Changing power source from USB (3.3 V) to batteries (approximately 3 V) could drastically reduce the contrast. Fortunately, the LCD driver supports adjustable contrast. The specific instruction can be found in the LCD user's guide. The MSP-EXP430F5529 software also provides the function to adjust the contrast using the wheel (see Section 2.8).
Verify that all jumpers are installed correctly and the 14-pin JTAG cable are properly connected.