SLAU298A November   2009  – May 2021

 

  1.   Trademarks
  2. 1ADS8555EVM-PDK Overview
    1. 1.1 ADS8555EVM-PDK Features
    2. 1.2 ADS8555EVM Features
  3. 2EVM Analog Interface
    1. 2.1 ADC Supply, Input, Voltage Reference, and Digital Connections
    2. 2.2 ADC Amplifier Drive
  4. 3Digital Interface
    1. 3.1 Parallel Interface
    2. 3.2 Serial Interface (SPI)
    3. 3.3 I2C Bus and EEPROM
    4. 3.4 Connections to the PHI Connector
  5. 4Power Supplies
    1. 4.1 External Power Connections and Test Points
    2. 4.2 Low-Dropout Regulator (TPS7A3001 for HVSS)
    3. 4.3 Low-Dropout Regulator (TPS7A4700 for AVDD, HVDD)
  6. 5Installing the ADS8555EVM Software
  7. 6ADS8555EVM Operation
    1. 6.1 Connecting the Hardware and Running the GUI
    2. 6.2 Jumper Settings for the ADS8555EVM
    3. 6.3 Modifying Hardware and Using Software to Evaluate Other Devices in the Family
    4. 6.4 EVM GUI Global Settings for ADC Control and Registers
    5. 6.5 Time Domain Display
    6. 6.6 Frequency Domain Display
    7. 6.7 Histogram Display
  8. 7Bill of Materials, Layout, and Schematics
    1. 7.1 Bill of Materials
    2. 7.2 Board Layout
    3. 7.3 Schematics
  9. 8Revision History

Modifying Hardware and Using Software to Evaluate Other Devices in the Family

The ADS8555 is part of a family of related devices. This EVM hardware and software support the entire family because all the devices are pin-for-pin compatible. The Table 6-2 lists other compatible devices in the family. The following procedure shows how to modify the hardware and software to evaluate the other devices in this family.

  1. Desolder the ADS8555 and replace this device with the device you want to evaluate.
  2. Enable the EEPROM for writing. This process is done by changing switch S2 to the WR_EN (top) position using tweezers. Figure 6-3 details this process.
  3. Connect the EVM and start the GUI as described in Figure 6-2.
  4. Under the Tools menu in Figure 6-4, select Load EEPROM to load the EEPROM according to the device that is currently installed. When this procedure is successfully completed, the status bar at the top of the software updates according to the device installed on the hardware.
Table 6-2 Compatible Devices
DEVICE RESOLUTION PARALLEL DATA RATE SERIAL DATA RATE OTHER FEATURE
ADS8555 16 630 450 Does not have partial power-down mode
ADS8556 16 630 450 —
ADS8557 14 670 470 —
ADS8558 12 730 500 —
GUID-20210429-CA0I-RWP6-R40R-DNFJSQ4JBBDB-low.gif Figure 6-3 Enable EEPROM for Writing
GUID-20210429-CA0I-PVKC-5XJN-XGHQWKWHP3TH-low.gif Figure 6-4 Configure EEPROM and Software for the New Device