SLAU298A November 2009 – May 2021
Figure 2-1 shows the decoupling on AVDD, BVDD, HVDD, and HVSS and the voltage reference. The decoupling capacitors match the recommendations in the ADS8555 data sheet. The layout (see Figure 7-1) uses the shortest possible connections to the decoupling capacitors and connects the ground end to the GND plane using vias. The ADS8555 can use an external or internal voltage reference. This reference can be selected by changing the position of JP06 to INT for internal or EXT for external. Figure 2-1 also shows the analog input signal and digital signal connections.
Figure 2-1 ADC Signal and Supply Connection