SLAU298A November   2009  – May 2021

 

  1.   Trademarks
  2. 1ADS8555EVM-PDK Overview
    1. 1.1 ADS8555EVM-PDK Features
    2. 1.2 ADS8555EVM Features
  3. 2EVM Analog Interface
    1. 2.1 ADC Supply, Input, Voltage Reference, and Digital Connections
    2. 2.2 ADC Amplifier Drive
  4. 3Digital Interface
    1. 3.1 Parallel Interface
    2. 3.2 Serial Interface (SPI)
    3. 3.3 I2C Bus and EEPROM
    4. 3.4 Connections to the PHI Connector
  5. 4Power Supplies
    1. 4.1 External Power Connections and Test Points
    2. 4.2 Low-Dropout Regulator (TPS7A3001 for HVSS)
    3. 4.3 Low-Dropout Regulator (TPS7A4700 for AVDD, HVDD)
  6. 5Installing the ADS8555EVM Software
  7. 6ADS8555EVM Operation
    1. 6.1 Connecting the Hardware and Running the GUI
    2. 6.2 Jumper Settings for the ADS8555EVM
    3. 6.3 Modifying Hardware and Using Software to Evaluate Other Devices in the Family
    4. 6.4 EVM GUI Global Settings for ADC Control and Registers
    5. 6.5 Time Domain Display
    6. 6.6 Frequency Domain Display
    7. 6.7 Histogram Display
  8. 7Bill of Materials, Layout, and Schematics
    1. 7.1 Bill of Materials
    2. 7.2 Board Layout
    3. 7.3 Schematics
  9. 8Revision History

EVM GUI Global Settings for ADC Control and Registers

Figure 6-5 shows the Register Map page. This page can only be accessed by selecting Software device mode. Editing the CONFIG_REG configures the different ranges and voltage references available on the ADS8555. See the ADS8555 data sheet for register field details. The left hand side of this GUI contains important configurations such as interface selection, device mode, range selection, and sampling rate. These controls are always available on the left hand side of the GUI regardless of which page is selected. Also, if Hardware mode is used, the hardware input select pins on the device are set according the controls on the left hand side. For example, when in hardware mode if the Parallel Interface is selected, than the PAR/SER pin on the device is driven low by the PHI to select parallel interface mode.

GUID-20210426-CA0I-RGLQ-XDSJ-T1ZVMBXGN6MF-low.gif Figure 6-5 EVM GUI Global Settings for ADC Control and Registers