SFFS983 August 2025 MSPM0G1518 , MSPM0G1519 , MSPM0G3518 , MSPM0G3519
In the case where timing parameters of safety-critical inputs are measured, two or more pins can be connected to the same signal (redundancy), and the measured parameters (in different timer instances) can be compared to determine if the parameters are within the acceptable range. Input capture must be done on different timer instances. This covers faults in the clock divider as the measured timing parameters deviate from the expected values on the second instance.