DLPU115 January 2022 DLPC3421
The read parameter specifies the splash screen for which the header parameters are returned. If a splash screen value is provided for an unavailable splash screen, this is considered an error (invalid command parameter value – communication status).
| Parameter Bytes | Description |
|---|---|
| Byte 1 | Splash screen reference number (integer) |