SLUS652E March 2005 – April 2020 UCD8220
PRODUCTION DATA.
请参考 PDF 数据表获取器件具体的封装图。
The UCD8220 device contains drivers that can deliver high current into a MOSFET gate for a period of several hundred nanoseconds. High-peak current is required to turn on a MOSFET. To turn off a MOSFET, the driver is required to sink a similar amount of current to ground. This cycle repeats at the operating frequency of the power device.
For additional information on the current required to drive a power MOSFET and other capacitive-input switching devices, see (5) in the Related Documentation section.
When a driver device is tested with a discrete, capacitive load, calculating the power that is required from the bias supply is fairly simple. Use Equation 1 to calculate the energy that must be transferred from the bias supply to charge the capacitor.
where
An equal amount of energy is transferred to ground when the capacitor is discharged. This transfer of energy results in a power loss which is calculated with Equation 2.
where
This power is dissipated in the resistive elements of the circuit. Thus, with no external resistor between the driver and gate, this power is dissipated inside the driver. Half of the total power is dissipated when the capacitor is charged, and the other half is dissipated when the capacitor is discharged.
Use Equation 3 to calculate the power loss with the following values: VDD = 12 V, CLOAD = 2.2 nF, and f = 300 kHz.
Use Equation 4 to calculate the current with a 12-V supply.