ZHCSC70D December 2013 – December 2021 DAC7750 , DAC8750
PRODUCTION DATA
The DACx750 provides access to internal nodes of the circuit; see Figure 9-2. Place capacitors on these pins and AVDD to form a filter on the output current, reducing bandwidth and the slew rate of the output, especially useful for driving inductive loads. However, to achieve large reductions in slew rate, use the programmable slew rate to avoid having to use large capacitors. Even in that case, use the capacitors on CAP1 and CAP2 to smooth out the stairsteps caused by the digital code changes as shown in Figure 8-6. However, note that power supply ripple also couples into the devices through these capacitors.
Figure 8-6 IOUT vs Time for Different Cap Values on CAP1 and CAP2