| 15 |
FIFO_ZEROS_DATA |
R/W |
1 |
When asserted FIFO errors zero the data out of the JESD block. For test purposes this could be turned off to allow test patterns in the FIFO. |
| 14:13 |
NOT USED |
R/W |
000 |
Not Used |
| 12 |
SRDS_FIFO_ALM_CLR |
R/W |
0 |
Set to 1 to clear FIFO errors. Must be set to 0 for proper FIFO operation |
| 11 |
Not used |
R/W |
0 |
Not used |
| 10:8 |
FIFO_OFFSET |
R/W |
0000 |
Used to set the difference between read and write pointers in the JESD FIFO. |
| 7:1 |
Reserved |
R/W |
0 |
Reserved |
| 0 |
SPI_TXENABLE |
R/W |
0 |
When asserted the internal value of txenable = '1' |