| 15:8 |
MATCH_DATA |
R/W |
0x1C |
The character to match for buffer release. Normally it is a /R/=/K28.0/-0x1C but with these bits the user can program the value. |
| 7 |
MATCH_SPECIFIC |
R/W |
1 |
Match a specific charater to start the JESD buffering when asserted; otherwise the first non-K will start the buffering. |
| 6 |
MATCH_CTRL |
R/W |
1 |
When asserted the match character is a CONTROL character instead of a DATA character. |
| 5 |
NO_LANE_SYNC |
R/W |
0 |
Assert if the TX side does not support lane initialization. This way the RX won’t flag errors in the configuration portion of the ILA. |
| 4:2 |
Not Used |
R/W |
000 |
Not Used |
| 1 |
MIN_LATENCY_ENA |
R/W |
0 |
Enable minimum latency when set. This is needed for subclass 0 support. |
| 0 |
JESD_COMMAALIGN_ENA |
R/W |
1 |
When asserted the JESD block SERDES comma align signal will be added with the SERDES ALIGN bit(0) to control when to shut off comma alignment. When this bit is deasserted; then the programmed bit(spi_config62(11)) is the only control. |