ZHCSNS4C April 2021 – September 2022 ADS127L11
PRODUCTION DATA
In 3-wire SPI mode, an unintended SCLK can misalign the frame, resulting in loss of frame synchronization to the ADC. As shown in Figure 8-40, the SPI is resynchronized without requiring an ADC reset by sending an SPI reset pattern. The reset pattern is a minimum of 63 consecutive 1s followed by one 0 at the 64th SCLK. The 65th SCLK starts a new SPI frame. Optionally, the ADC can be completely reset by toggling RESET or by the reset pattern shown in the Section 8.4.5.3 section.
Figure 8-40 3-Wire Mode SPI Reset Pattern