ZHCSBT2G November 2012 – October 2017 66AK2H06 , 66AK2H12 , 66AK2H14
PRODUCTION DATA.
The 66AK2Hxx device has a set of registers that are used to control the status of its peripherals. These registers are shown in Table 10-30.
| ADDRESS START | ADDRESS END | SIZE | ACRONYM | DESCRIPTION |
|---|---|---|---|---|
| 0x02620000 | 0x02620007 | 8B | Reserved | |
| 0x02620008 | 0x02620017 | 16B | Reserved | |
| 0x02620018 | 0x0262001B | 4B | JTAGID | See Section 10.2.3.3 |
| 0x0262001C | 0x0262001F | 4B | Reserved | |
| 0x02620020 | 0x02620023 | 4B | DEVSTAT | See Section 10.2.3.1 |
| 0x02620024 | 0x02620037 | 20B | Reserved | |
| 0x02620038 | 0x0262003B | 4B | KICK0 | See Section 10.2.3.4 |
| 0x0262003C | 0x0262003F | 4B | KICK1 | |
| 0x02620040 | 0x02620043 | 4B | DSP_BOOT_ADDR0 | The boot address for C66x CorePac0. See Section 10.2.3.5 |
| 0x02620044 | 0x02620047 | 4B | DSP_BOOT_ADDR1 | The boot address for C66x CorePac1. See Section 10.2.3.5 |
| 0x02620048 | 0x0262004B | 4B | DSP_BOOT_ADDR2 | The boot address for C66x CorePac2. See Section 10.2.3.5 |
| 0x0262004C | 0x0262004F | 4B | DSP_BOOT_ADDR3 | The boot address for C66x CorePac3. See Section 10.2.3.5 |
| 0x02620050 | 0x02620053 | 4B | DSP_BOOT_ADDR4 | The boot address for C66x CorePac4 (66AK2H14/12 only). See Section 10.2.3.5 |
| 0x02620054 | 0x02620057 | 4B | DSP_BOOT_ADDR5 | The boot address for C66x CorePac5 (66AK2H14/12 only). See Section 10.2.3.5 |
| 0x02620058 | 0x0262005B | 4B | DSP_BOOT_ADDR6 | The boot address for C66x CorePac6 (66AK2H14/12 only). See Section 10.2.3.5 |
| 0x0262005C | 0x0262005F | 4B | DSP_BOOT_ADDR7 | The boot address for C66x CorePac7 (66AK2H14/12 only). See Section 10.2.3.5 |
| 0x02620060 | 0x026200DF | 128B | Reserved | |
| 0x026200E0 | 0x0262010F | 48B | Reserved | |
| 0x02620110 | 0x02620117 | 8B | MACID | See Section 11.17 |
| 0x02620118 | 0x0262012F | 24B | Reserved | |
| 0x02620130 | 0x02620133 | 4B | LRSTNMIPINSTAT_CLR | See Section 10.2.3.7 |
| 0x02620134 | 0x02620137 | 4B | RESET_STAT_CLR | See Section 10.2.3.9 |
| 0x02620138 | 0x0262013B | 4B | Reserved | |
| 0x0262013C | 0x0262013F | 4B | BOOTCOMPLETE | See Section 10.2.3.10 |
| 0x02620140 | 0x02620143 | 4B | Reserved | |
| 0x02620144 | 0x02620147 | 4B | RESET_STAT | See Section 10.2.3.8 |
| 0x02620148 | 0x0262014B | 4B | LRSTNMIPINSTAT | See Section 10.2.3.6 |
| 0x0262014C | 0x0262014F | 4B | DEVCFG | See Section 10.2.3.2 |
| 0x02620150 | 0x02620153 | 4B | PWRSTATECTL | See Section 10.2.3.11 |
| 0x02620154 | 0x02620157 | 4B | Reserved | |
| 0x02620158 | 0x0262015B | 4B | Reserved | |
| 0x0262015C | 0x0262015F | 4B | Reserved | |
| 0x02620160 | 0x02620160 | 4B | Reserved | |
| 0x02620164 | 0x02620167 | 4B | Reserved | |
| 0x02620168 | 0x0262016B | 4B | Reserved | |
| 0x0262016C | 0x0262017F | 20B | Reserved | |
| 0x02620180 | 0x02620183 | 4B | SmartReflex Class0 | See Section 11.2.4 |
| 0x02620184 | 0x0262018F | 12B | Reserved | |
| 0x02620190 | 0x02620193 | 4B | Reserved | |
| 0x02620194 | 0x02620197 | 4B | Reserved | |
| 0x02620198 | 0x0262019B | 4B | Reserved | |
| 0x0262019C | 0x0262019F | 4B | Reserved | |
| 0x026201A0 | 0x026201A3 | 4B | Reserved | |
| 0x026201A4 | 0x026201A7 | 4B | Reserved | |
| 0x026201A8 | 0x026201AB | 4B | Reserved | |
| 0x026201AC | 0x026201AF | 4B | Reserved | |
| 0x026201B0 | 0x026201B3 | 4B | Reserved | |
| 0x026201B4 | 0x026201B7 | 4B | Reserved | |
| 0x026201B8 | 0x026201BB | 4B | Reserved | |
| 0x026201BC | 0x026201BF | 4B | Reserved | |
| 0x026201C0 | 0x026201C3 | 4B | Reserved | |
| 0x026201C4 | 0x026201C7 | 4B | Reserved | |
| 0x026201C8 | 0x026201CB | 4B | Reserved | |
| 0x026201CC | 0x026201CF | 4B | Reserved | |
| 0x026201D0 | 0x026201FF | 48B | Reserved | |
| 0x02620200 | 0x02620203 | 4B | NMIGR0 | See Section 10.2.3.12 |
| 0x02620204 | 0x02620207 | 4B | NMIGR1 | |
| 0x02620208 | 0x0262020B | 4B | NMIGR2 | |
| 0x0262020C | 0x0262020F | 4B | NMIGR3 | |
| 0x02620210 | 0x02620213 | 4B | NMIGR4 (66AK2H14/12 only) | |
| 0x02620214 | 0x02620217 | 4B | NMIGR5 (66AK2H14/12 only) | |
| 0x02620218 | 0x0262021B | 4B | NMIGR6 (66AK2H14/12 only) | |
| 0x0262021C | 0x0262021F | 4B | NMIGR7 (66AK2H14/12 only) | |
| 0x02620220 | 0x0262023F | 32B | Reserved | |
| 0x02620240 | 0x02620243 | 4B | IPCGR0 | See Section 10.2.3.13 |
| 0x02620244 | 0x02620247 | 4B | IPCGR1 | |
| 0x02620248 | 0x0262024B | 4B | IPCGR2 | |
| 0x0262024C | 0x0262024F | 4B | IPCGR3 | |
| 0x02620250 | 0x02620253 | 4B | IPCGR4 | |
| 0x02620254 | 0x02620257 | 4B | IPCGR5 | |
| 0x02620258 | 0x0262025B | 4B | IPCGR6 | |
| 0x0262025C | 0x0262025F | 4B | IPCGR7 | |
| 0x02620260 | 0x02620263 | 4B | IPCGR8 | |
| 0x02620264 | 0x02620267 | 4B | IPCGR9 | |
| 0x02620268 | 0x0262026B | 4B | IPCGR10 | |
| 0x0262026C | 0x0262026F | 4B | IPCGR11 | |
| 0x02620270 | 0x0262027B | 12B | Reserved | |
| 0x0262027C | 0x0262027F | 4B | IPCGRH | See Section 10.2.3.15 |
| 0x02620280 | 0x02620283 | 4B | IPCAR0 | See Section 10.2.3.14 |
| 0x02620284 | 0x02620287 | 4B | IPCAR1 | |
| 0x02620288 | 0x0262028B | 4B | IPCAR2 | |
| 0x0262028C | 0x0262028F | 4B | IPCAR3 | |
| 0x02620290 | 0x02620293 | 4B | IPCAR4 | |
| 0x02620294 | 0x02620297 | 4B | IPCAR5 | |
| 0x02620298 | 0x0262029B | 4B | IPCAR6 | |
| 0x0262029C | 0x0262029F | 4B | IPCAR7 | |
| 0x026202A0 | 0x026202A3 | 4B | IPCAR8 | |
| 0x026202A4 | 0x026202A7 | 4B | IPCAR9 | |
| 0x026202A8 | 0x026202AB | 4B | IPCAR10 | |
| 0x026202AC | 0x026202AF | 4B | IPCAR11 | |
| 0x026202B0 | 0x026202BB | 12B | Reserved | |
| 0x026202BC | 0x026202BF | 4B | IPCARH | See Section 10.2.3.16 |
| 0x026202C0 | 0x026202FF | 64B | Reserved | |
| 0x02620300 | 0x02620303 | 4B | TINPSEL | See Section 10.2.3.17 |
| 0x02620304 | 0x02620307 | 4B | TOUTPSEL | See Section 10.2.3.18 |
| 0x02620308 | 0x0262030B | 4B | RSTMUX0 | See Section 10.2.3.19 |
| 0x0262030C | 0x0262030F | 4B | RSTMUX1 | |
| 0x02620310 | 0x02620313 | 4B | RSTMUX2 | |
| 0x02620314 | 0x02620317 | 4B | RSTMUX3 | |
| 0x02620318 | 0x0262031B | 4B | RSTMUX4 | |
| 0x0262031C | 0x0262031F | 4B | RSTMUX5 | |
| 0x02620320 | 0x02620323 | 4B | RSTMUX6 | |
| 0x02620324 | 0x02620327 | 4B | RSTMUX7 | |
| 0x02620328 | 0x0262032B | 4B | RSTMUX8 | |
| 0x0262032C | 0x0262032F | 4B | RSTMUX9 | |
| 0x02620330 | 0x02620333 | 4B | RSTMUX10 | |
| 0x02620334 | 0x02620337 | 4B | RSTMUX11 | |
| 0x02620338 | 0x0262034F | 4B | Reserved | |
| 0x02620350 | 0x02620353 | 4B | MAINPLLCTL0 | See Section 11.5 |
| 0x02620354 | 0x02620357 | 4B | MAINPLLCTL1 | |
| 0x02620358 | 0x0262035B | 4B | PASSPLLCTL0 | See Section 11.7 |
| 0x0262035C | 0x0262035F | 4B | PASSPLLCTL1 | |
| 0x02620360 | 0x02620363 | 4B | DDR3APLLCTL0 | See Section 11.6 |
| 0x02620364 | 0x02620367 | 4B | DDR3APLLCTL1 | |
| 0x02620368 | 0x0262036B | 4B | DDR3BPLLCTL0 | See Section 11.6 |
| 0x0262036C | 0x0262036F | 4B | DDR3BPLLCTL1 | |
| 0x02620370 | 0x02620373 | 4B | ARMPLLCTL0 | See Section 10.1.4.1 |
| 0x02620374 | 0x02620377 | 4B | ARMPLLCTL1 | |
| 0x02620378 | 0x0262039B | 132B | Reserved | |
| 0x0262039C | 0x0262039F | 4B | Reserved | |
| 0x02620400 | 0x02620403 | 4B | ARMENDIAN_CFG0_0 | See Section 10.2.3.21 |
| 0x02620404 | 0x02620407 | 4B | ARMENDIAN_CFG0_1 | |
| 0x02620408 | 0x0262040B | 4B | ARMENDIAN_CFG0_2 | |
| 0x0262040C | 0x026205FF | 62B | Reserved | |
| 0x02620600 | 0x026206FF | 256B | Reserved | |
| 0x02620700 | 0x02620703 | 4B | CHIP_MISC_CTL0 | See Section 10.2.3.24 |
| 0x02620704 | 0x0262070F | 12B | Reserved | |
| 0x02620710 | 0x02620713 | 4B | SYSENDSTAT | See Section 10.2.3.26 |
| 0x02620714 | 0x02620717 | 4B | Reserved | |
| 0x02620718 | 0x0262071B | 4B | Reserved | |
| 0x0262071C | 0x0262071F | 4B | Reserved | |
| 0x02620720 | 0x0262072F | 16B | Reserved | |
| 0x02620730 | 0x02620733 | 4B | SYNECLK_PINCTL | See Section 10.2.3.27 |
| 0x02620734 | 0x02620737 | 4B | Reserved | |
| 0x02620738 | 0x0262074F | 24B | USB_PHY_CTL | See Section 10.2.3.28 |
| 0x02620750 | 0x026207FF | 176B | Reserved | |
| 0x02620800 | 0x02620C7B | 1148B | Reserved | |
| 0x02620C7C | 0x02620C7F | 4B | CHIP_MISC_CTL1 | See Section 10.2.3.25 |
| 0x02620C80 | 0x02620C97 | 24B | Reserved | |
| 0x02620C90
(silicon revisions 2.0, 3.0, and 3.1) |
0x02620C93
(silicon revisions 2.0, 3.0, and 3.1) |
4B | DEVSPEED | See Section 10.2.3.20 |
| 0x02620C98
(silicon revision 1.1, 1.0) |
0x02620C9B
(silicon revision 1.1, 1.0) |
4B | DEVSPEED | See Section 10.2.3.20 |
| 0x02620C9C | 0x02620FFF | 868B | Reserved |